problem aboutMCF52211's RTC module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem aboutMCF52211's RTC module

ソリューションへジャンプ
2,255件の閲覧回数
bluehacker
Contributor III
I want to use mcf52211 to develop one product. I want to use its RTC module,but I hope it can keep running even when VDD,VDDPLL is power down, the mcf52211 has VSTBY pin,so I think use a battery backup power to VSTBY pin. my question is whether the method works?
thanks!
ラベル(1)
0 件の賞賛
返信
1 解決策
1,614件の閲覧回数
mjbcswitzerland
Specialist V
Hi

The RTC can be used together with 32kHz crystal and battery backup.

See also http://www.utasker.com/forum/index.php?topic=256.0

Note that the 32kHz crystal shares pins with UART0, meaning that UART0 can no longer be used if the RTC crystal is required. This restriction is removed in the M5225X family, where there are dedicated 32kHz RTC crystal inputs.

Regards

Mark


www.uTasker.com



元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,614件の閲覧回数
mjbcswitzerland
Specialist V
Hi

The RTC can be used together with 32kHz crystal and battery backup.

See also http://www.utasker.com/forum/index.php?topic=256.0

Note that the 32kHz crystal shares pins with UART0, meaning that UART0 can no longer be used if the RTC crystal is required. This restriction is removed in the M5225X family, where there are dedicated 32kHz RTC crystal inputs.

Regards

Mark


www.uTasker.com



0 件の賞賛
返信