about M52235EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about M52235EVB

3,800 Views
gloin
Contributor I

I m newbie in Freescale products, I d like to ask does the M52235EVB kit contain a debugger or programmer? It is written that it includes a wiggler cable only. I m confused with this. Could someone enlighten me, which debugger and/or programmer do I need for this board? Any help will be appreciated..

regards,

Gloin

Labels (1)
0 Kudos
Reply
2 Replies

1,520 Views
mjbcswitzerland
Specialist V

Hi Gloin

The M52235EVB ($299) comes with a 128k limited Codewarrior version.
It has also a USB Coldfire MULTILINK from P+E so you have everything which you need to work with the board.

There is also a cheaper M52233DEMO (for $99) which comes with the BDM integrated into the board.

Check out also the following posting:
http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=274

Regards

Mark Butcher
www.mjbc.ch

0 Kudos
Reply

1,520 Views
J2MEJediMaster
Specialist I
I've looked at the write-up for this particular board (found here), and it indicates that the kit comes with Codewarrior Special Edition, which should allow you to compile, download, and debug apps on the board.

---Tom
0 Kudos
Reply