about M52235EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about M52235EVB

3,814件の閲覧回数
gloin
Contributor I

I m newbie in Freescale products, I d like to ask does the M52235EVB kit contain a debugger or programmer? It is written that it includes a wiggler cable only. I m confused with this. Could someone enlighten me, which debugger and/or programmer do I need for this board? Any help will be appreciated..

regards,

Gloin

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,534件の閲覧回数
mjbcswitzerland
Specialist V

Hi Gloin

The M52235EVB ($299) comes with a 128k limited Codewarrior version.
It has also a USB Coldfire MULTILINK from P+E so you have everything which you need to work with the board.

There is also a cheaper M52233DEMO (for $99) which comes with the BDM integrated into the board.

Check out also the following posting:
http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=274

Regards

Mark Butcher
www.mjbc.ch

0 件の賞賛
返信

1,534件の閲覧回数
J2MEJediMaster
Specialist I
I've looked at the write-up for this particular board (found here), and it indicates that the kit comes with Codewarrior Special Edition, which should allow you to compile, download, and debug apps on the board.

---Tom
0 件の賞賛
返信