Using BDM Connector, SingleStep Debugger, and M547xEVB Lite Development Kit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using BDM Connector, SingleStep Debugger, and M547xEVB Lite Development Kit

3,295 次查看
Linux
Contributor I
I am currently using the SingleStep debugger connected to the M547xEVB Lite Development Kit via a BDM connector.

Occasionally, the debugger will display the following message.

.....@: error: There was no DTACK/TEA response for a longword-sized write access at 5:20002000.
.....It is possible that the address is configured for an external DTACK when there isn't any.
.....It is also possible that this is an invalid address,
.....but the bus monitor has not been enabled in FREEZE mode.
.....We tried asserting TEA, but that did not work (TEA not present on BDM connector?)

When the above message appears, the debugger immediately loses communication with the M547xEVB Lite Development Kit.

How can I set up the debugger and/or its script/configuration files to prevent the above message from appearing?
标签 (1)
0 项奖励
回复
1 回复

1,636 次查看
mnorman
NXP Employee
NXP Employee
What can you tell us about this access to 0x20002000?  Is that a valid address in your setup?
0 项奖励
回复