Using BDM Connector, SingleStep Debugger, and M547xEVB Lite Development Kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using BDM Connector, SingleStep Debugger, and M547xEVB Lite Development Kit

3,285件の閲覧回数
Linux
Contributor I
I am currently using the SingleStep debugger connected to the M547xEVB Lite Development Kit via a BDM connector.

Occasionally, the debugger will display the following message.

.....@: error: There was no DTACK/TEA response for a longword-sized write access at 5:20002000.
.....It is possible that the address is configured for an external DTACK when there isn't any.
.....It is also possible that this is an invalid address,
.....but the bus monitor has not been enabled in FREEZE mode.
.....We tried asserting TEA, but that did not work (TEA not present on BDM connector?)

When the above message appears, the debugger immediately loses communication with the M547xEVB Lite Development Kit.

How can I set up the debugger and/or its script/configuration files to prevent the above message from appearing?
ラベル(1)
0 件の賞賛
返信
1 返信

1,626件の閲覧回数
mnorman
NXP Employee
NXP Employee
What can you tell us about this access to 0x20002000?  Is that a valid address in your setup?
0 件の賞賛
返信