Using BDM Connector, SingleStep Debugger, and M547xEVB Lite Development Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using BDM Connector, SingleStep Debugger, and M547xEVB Lite Development Kit

3,238 Views
Linux
Contributor I
I am currently using the SingleStep debugger connected to the M547xEVB Lite Development Kit via a BDM connector.

Occasionally, the debugger will display the following message.

.....@: error: There was no DTACK/TEA response for a longword-sized write access at 5:20002000.
.....It is possible that the address is configured for an external DTACK when there isn't any.
.....It is also possible that this is an invalid address,
.....but the bus monitor has not been enabled in FREEZE mode.
.....We tried asserting TEA, but that did not work (TEA not present on BDM connector?)

When the above message appears, the debugger immediately loses communication with the M547xEVB Lite Development Kit.

How can I set up the debugger and/or its script/configuration files to prevent the above message from appearing?
Labels (1)
0 Kudos
Reply
1 Reply

1,579 Views
mnorman
NXP Employee
NXP Employee
What can you tell us about this access to 0x20002000?  Is that a valid address in your setup?
0 Kudos
Reply