U-boot problem with a mcf5485 processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-boot problem with a mcf5485 processor

ソリューションへジャンプ
2,469件の閲覧回数
raulen
Contributor III
Hello everybody!
 
I am trying to port U-boot to my custom board which has a mcf5485 processor.
 
First of all I run the U-boot in an evaluation board (M5484Lite evb) and it worked perfectly. Then I tried to do it with my custom board (after modifying and adding the right files). The problem seems to be in the internal SRAM at the beginning of the code (start.S). I enabled some LEDS and after several tries, I found out I couldn't have access to the internal SRAM, in spite of having the same code to the evaluation board.
 
However, if I use an external sram, the u-boot goes (not completely, but at least till I know it should without doing changes).
Regarding the datasheet and the code, I have to configure the RAMBAR0 and RAMBAR1 of the internal SRAM. From this moment, I should have access, but if I try to write in the memory, it crashes (I can observe that because the leds).
 
Does anyone ported the U-boot for their custom boards?
Some help would be appreciated.
Thanks.
ラベル(1)
0 件の賞賛
返信
1 解決策
1,633件の閲覧回数
raulen
Contributor III
Upps! I realised it was an error mapping... it works perfectly!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,634件の閲覧回数
raulen
Contributor III
Upps! I realised it was an error mapping... it works perfectly!
0 件の賞賛
返信