U-boot problem with a mcf5485 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-boot problem with a mcf5485 processor

Jump to solution
2,505 Views
raulen
Contributor III
Hello everybody!
 
I am trying to port U-boot to my custom board which has a mcf5485 processor.
 
First of all I run the U-boot in an evaluation board (M5484Lite evb) and it worked perfectly. Then I tried to do it with my custom board (after modifying and adding the right files). The problem seems to be in the internal SRAM at the beginning of the code (start.S). I enabled some LEDS and after several tries, I found out I couldn't have access to the internal SRAM, in spite of having the same code to the evaluation board.
 
However, if I use an external sram, the u-boot goes (not completely, but at least till I know it should without doing changes).
Regarding the datasheet and the code, I have to configure the RAMBAR0 and RAMBAR1 of the internal SRAM. From this moment, I should have access, but if I try to write in the memory, it crashes (I can observe that because the leds).
 
Does anyone ported the U-boot for their custom boards?
Some help would be appreciated.
Thanks.
Labels (1)
0 Kudos
Reply
1 Solution
1,669 Views
raulen
Contributor III
Upps! I realised it was an error mapping... it works perfectly!

View solution in original post

0 Kudos
Reply
1 Reply
1,670 Views
raulen
Contributor III
Upps! I realised it was an error mapping... it works perfectly!
0 Kudos
Reply