MCF5475CFE PCI Controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF5475CFE PCI Controller

1,702 Views
mniuser
Contributor I
For a breadboard we are designing, we are using 2 Fire Engine modules mounted on a host board. The final design will be using the PCI bus for communication between Coldfire processors. I would like to connect both Fire Engine MCF5475s to the same PCI bus on the host board, but have encountered two issues.   
1.  The PCI clock for the FE is supplied by the clock on board.   I don't see a way to provide an outside clock source, so cannot put both processors on the same PCI clock source.
2.  The PCI_IDSEL line is hardwired to PCI_AD16.   (This is used for Type 0 Configuration).  I think that this can be overcome by software though, which would be okay for breadboard purposes.
 
Any suggestions on how to get around the clock issue?
Labels (1)
0 Kudos
Reply
1 Reply

1,259 Views
kmahan
Contributor I
My comment isn't specifically related to you're question, but since you are using PCI on the fireengines please read the release note (the section on PCI) in the latest BSP.
0 Kudos
Reply