MCF52259 battery backed up RAM section

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF52259 battery backed up RAM section

Jump to solution
1,692 Views
drummer
Contributor IV

I read somewhere that half of the internal ram may be preserved with a battery during power down.

I have searched through my documentation for this but can't find anything.

Is this true or am I dreaming?

If so, what half is preserved?

Labels (1)
0 Kudos
Reply
1 Solution
1,436 Views
mjbcswitzerland
Specialist V

Hi

 

"Vstby backs up the first 16K of SRAM and the RTC when the main power is shut down".

 

See https://community.freescale.com/thread/51895 and also page 5 of the Data Sheet for the M52259.

 

Regards

 

Mark

 

View solution in original post

0 Kudos
Reply
2 Replies
1,437 Views
mjbcswitzerland
Specialist V

Hi

 

"Vstby backs up the first 16K of SRAM and the RTC when the main power is shut down".

 

See https://community.freescale.com/thread/51895 and also page 5 of the Data Sheet for the M52259.

 

Regards

 

Mark

 

0 Kudos
Reply
1,436 Views
drummer
Contributor IV

Thanks !

0 Kudos
Reply