MCF52259 battery backed up RAM section

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52259 battery backed up RAM section

ソリューションへジャンプ
1,690件の閲覧回数
drummer
Contributor IV

I read somewhere that half of the internal ram may be preserved with a battery during power down.

I have searched through my documentation for this but can't find anything.

Is this true or am I dreaming?

If so, what half is preserved?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,434件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

"Vstby backs up the first 16K of SRAM and the RTC when the main power is shut down".

 

See https://community.freescale.com/thread/51895 and also page 5 of the Data Sheet for the M52259.

 

Regards

 

Mark

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,435件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

"Vstby backs up the first 16K of SRAM and the RTC when the main power is shut down".

 

See https://community.freescale.com/thread/51895 and also page 5 of the Data Sheet for the M52259.

 

Regards

 

Mark

 

0 件の賞賛
返信
1,434件の閲覧回数
drummer
Contributor IV

Thanks !

0 件の賞賛
返信