MCF52259 battery backed up RAM section

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCF52259 battery backed up RAM section

跳至解决方案
1,704 次查看
drummer
Contributor IV

I read somewhere that half of the internal ram may be preserved with a battery during power down.

I have searched through my documentation for this but can't find anything.

Is this true or am I dreaming?

If so, what half is preserved?

标签 (1)
0 项奖励
回复
1 解答
1,448 次查看
mjbcswitzerland
Specialist V

Hi

 

"Vstby backs up the first 16K of SRAM and the RTC when the main power is shut down".

 

See https://community.freescale.com/thread/51895 and also page 5 of the Data Sheet for the M52259.

 

Regards

 

Mark

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,449 次查看
mjbcswitzerland
Specialist V

Hi

 

"Vstby backs up the first 16K of SRAM and the RTC when the main power is shut down".

 

See https://community.freescale.com/thread/51895 and also page 5 of the Data Sheet for the M52259.

 

Regards

 

Mark

 

0 项奖励
回复
1,448 次查看
drummer
Contributor IV

Thanks !

0 项奖励
回复