MCF52211 PUCPAR quad or dual function ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCF52211 PUCPAR quad or dual function ?

跳至解决方案
2,561 次查看
MrBean
Contributor I

The MCF52211RM Rev.2 states that PUCPAR is a dual-fuction register (aka 4 bit)

 

Every header file for it that i've been able to find states that PUCPAR is quad function (aka 8 bit)

 

 

Does anyone know which is right ?

 

 

I have no MCF52211 board to try it on.

Maybe someone that has such a board would be so kind to find out.

标签 (1)
0 项奖励
回复
1 解答
1,475 次查看
mjbcswitzerland
Specialist V

Hi MrBean

 

The port PUC has quad function on the M5222X and the M5225X.

It has dual function on the M5221X and the M5223X.

 

Regards

 

Mark

 

 

www.uTasker.com

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,476 次查看
mjbcswitzerland
Specialist V

Hi MrBean

 

The port PUC has quad function on the M5222X and the M5225X.

It has dual function on the M5221X and the M5223X.

 

Regards

 

Mark

 

 

www.uTasker.com

 

0 项奖励
回复
1,475 次查看
MrBean
Contributor I
Thanx ! :smileyhappy:
0 项奖励
回复
1,475 次查看
MrBean
Contributor I

PS:

 

The MCF52211EVB software, and possibly all other example software from Freescale, defines a quad function PUCPAR in MCF52211_GPIO.h

 

 

0 项奖励
回复