MCF52211 PUCPAR quad or dual function ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52211 PUCPAR quad or dual function ?

ソリューションへジャンプ
3,606件の閲覧回数
MrBean
Contributor I

The MCF52211RM Rev.2 states that PUCPAR is a dual-fuction register (aka 4 bit)

 

Every header file for it that i've been able to find states that PUCPAR is quad function (aka 8 bit)

 

 

Does anyone know which is right ?

 

 

I have no MCF52211 board to try it on.

Maybe someone that has such a board would be so kind to find out.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,520件の閲覧回数
mjbcswitzerland
Specialist V

Hi MrBean

 

The port PUC has quad function on the M5222X and the M5225X.

It has dual function on the M5221X and the M5223X.

 

Regards

 

Mark

 

 

www.uTasker.com

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,521件の閲覧回数
mjbcswitzerland
Specialist V

Hi MrBean

 

The port PUC has quad function on the M5222X and the M5225X.

It has dual function on the M5221X and the M5223X.

 

Regards

 

Mark

 

 

www.uTasker.com

 

0 件の賞賛
返信
2,520件の閲覧回数
MrBean
Contributor I
Thanx ! :smileyhappy:
0 件の賞賛
返信
2,520件の閲覧回数
MrBean
Contributor I

PS:

 

The MCF52211EVB software, and possibly all other example software from Freescale, defines a quad function PUCPAR in MCF52211_GPIO.h

 

 

0 件の賞賛
返信