Help ID board With MCF5213 processor.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help ID board With MCF5213 processor.

5,976 次查看
petronm20
Contributor I

I have a box of these boards in my stock and cannot figure out if I need them or not, seriously can't find anything on them through my normal database.  I know it's a long shot but was wondering if anyone here can help me identify what this board goes to and/or is used for it runs on a Coldfire MCF5213 connects via USB by FTDI. I know this is not a normal question here but it seems like this chip is pretty specialized so thought I may get lucky posting a few photos of the board on here seeing if someone knows theboard or could point me in the right direction on where I should start searching.  Thanks in advance for any information.

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

5,799 次查看
TomE
Specialist II

It would help to work out what it is if you could post the part numbers of the other large chips on the board.

I suspect it is some sort of function add-on board for a printer.

Tom

0 项奖励
回复

5,799 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

It is not a MCF5213 evaluation board for sure.

There with HP logo, could be circuit board used for HP products.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复