Coldfire MCF5208

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Coldfire MCF5208

1,527 Views
avinashnagumant
Contributor I


Hi i am using Lantronix Xport pro which uses Coldfire MCF5208. We are working on a new programming interface in which we had to cross compile to run the software on uclinux. Can you help me with the toolchain and their location of this specific hardware.

 

GCC Compiler, achiever, linker and flags required for cross build ?

Labels (1)
0 Kudos
Reply
2 Replies

1,397 Views
miduo
NXP Employee
NXP Employee

Hi,

For uClinux application & binary, please make reference from:

uClinux -- Embedded Linux/Microcontroller Project -- ColdFire: Binaries

B.R.

Fang

0 Kudos
Reply

1,397 Views
yibbidy
Contributor V

You get the linux hosted tools here:

http://www.lantronix.com/ftp/Linux_SDK/SDK2_0_0_3/linux_sdk_2_0_0_3.iso

There is an developer guide document in the iso which tells you everything you need to know to set up the development environment and compile/program/debug the XPort Pro.

Regards,

Shaun

0 Kudos
Reply