HELLO! AM USING MICROCONTROLLER MCFEM 256, AND WOULD LIKE TO ACTIVATE POTEÇÃO AGAINST WRITING IN FLASH MEMORY! WILL SOMEONE CAN HELP ME?  I THANK THE ATTENTION !

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HELLO! AM USING MICROCONTROLLER MCFEM 256, AND WOULD LIKE TO ACTIVATE POTEÇÃO AGAINST WRITING IN FLASH MEMORY! WILL SOMEONE CAN HELP ME?  I THANK THE ATTENTION !

1,644 Views
rosimarsilvaper
Contributor I

HELLO! AM USING MICROCONTROLLER MCFEM 256, AND WOULD LIKE TO ACTIVATE POTEÇÃO AGAINST WRITING IN FLASH MEMORY! WILL SOMEONE CAN HELP ME?

I THANK THE ATTENTION !

Labels (1)
0 Kudos
Reply
2 Replies

1,525 Views
miduo
NXP Employee
NXP Employee

Hi,

This post should help you on this regard:

https://community.nxp.com/message/109662

0 Kudos
Reply

1,525 Views
TomE
Specialist II

"MCFEM 256"? Do you mean "MCF51EM256"?

Read:

3.4.3.4 Flash Protection Register (FxPROT and NVPROT)

Tom

0 Kudos
Reply