Trace and Profiling available with SmartDSP OS on the MCS8156

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Trace and Profiling available with SmartDSP OS on the MCS8156

跳至解决方案
2,388 次查看
mkrug
Contributor II

Hello,

 

I am just playing around with the MCS8156EVM Board. While checking the different options for the project wizard it seems to me that the option 'trace and profile' (step 7/7) is only available if SmartDSP OS (step 4/7) is set to 'no'. Is this true ? any reasons ? any workarounds to use the trace and profile functionality and SmartDSP in the same project ?

 

Best Regards

Markus

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,789 次查看
Irene
NXP Pro Support
NXP Pro Support

There is trace functionality for the MSC8156EVM with or without SmartDSPOS.  What version and build number of the tools are you using?  I just verified on the latest toolset and I was able to set trace and profile for MSC8156EVM for SmartDSPOS and without SmartDSPOS?

 

Regards,
Irene

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,790 次查看
Irene
NXP Pro Support
NXP Pro Support

There is trace functionality for the MSC8156EVM with or without SmartDSPOS.  What version and build number of the tools are you using?  I just verified on the latest toolset and I was able to set trace and profile for MSC8156EVM for SmartDSPOS and without SmartDSPOS?

 

Regards,
Irene

0 项奖励
回复
1,789 次查看
mkrug
Contributor II

Hi Irene,

 

thanks for the hint. I just updated everything that is preset in the 'availabe software sites' dialog box and afterwards I can choose SmartDSP OS and trace functionality in one project.

 

Best Regards

Markus

0 项奖励
回复