Trace and Profiling available with SmartDSP OS on the MCS8156

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trace and Profiling available with SmartDSP OS on the MCS8156

ソリューションへジャンプ
2,382件の閲覧回数
mkrug
Contributor II

Hello,

 

I am just playing around with the MCS8156EVM Board. While checking the different options for the project wizard it seems to me that the option 'trace and profile' (step 7/7) is only available if SmartDSP OS (step 4/7) is set to 'no'. Is this true ? any reasons ? any workarounds to use the trace and profile functionality and SmartDSP in the same project ?

 

Best Regards

Markus

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,783件の閲覧回数
Irene
NXP Pro Support
NXP Pro Support

There is trace functionality for the MSC8156EVM with or without SmartDSPOS.  What version and build number of the tools are you using?  I just verified on the latest toolset and I was able to set trace and profile for MSC8156EVM for SmartDSPOS and without SmartDSPOS?

 

Regards,
Irene

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,784件の閲覧回数
Irene
NXP Pro Support
NXP Pro Support

There is trace functionality for the MSC8156EVM with or without SmartDSPOS.  What version and build number of the tools are you using?  I just verified on the latest toolset and I was able to set trace and profile for MSC8156EVM for SmartDSPOS and without SmartDSPOS?

 

Regards,
Irene

0 件の賞賛
返信
1,783件の閲覧回数
mkrug
Contributor II

Hi Irene,

 

thanks for the hint. I just updated everything that is preset in the 'availabe software sites' dialog box and afterwards I can choose SmartDSP OS and trace functionality in one project.

 

Best Regards

Markus

0 件の賞賛
返信