I don't find DSP Library mentioned in "Kernel Examples for the StarCore SC3850 DSP Core" document

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I don't find DSP Library mentioned in "Kernel Examples for the StarCore SC3850 DSP Core" document

ソリューションへジャンプ
1,710件の閲覧回数
sogico
Contributor I

Hi all,

 

I've been reading the manual "Kernel Examples for the StarCore SC3850 DSP Core" and I'd like to find the examples that are mentioned in this document, about FFT, CRC. It is said in the text that the version which contains all related examples is v10.1.x, but I didn't find that version available online... I use CodeWarrior for StarCore version 10.2.9.

 

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,232件の閲覧回数
J2MEJediMaster
Specialist I

The last paragraph on the opening page of application note AN4207 "Kernel Examples for the StarCore
SC3850 DSP Core", states:

 

NOTE
The supporting software library is available
as a zip file under NDA only. Contact your
local sales office or representative for details.

 

NDA = non-disclosure agreement

 

So, you need to contact a Freescale representative to sign an agreement and then obtain the software.

 

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,233件の閲覧回数
J2MEJediMaster
Specialist I

The last paragraph on the opening page of application note AN4207 "Kernel Examples for the StarCore
SC3850 DSP Core", states:

 

NOTE
The supporting software library is available
as a zip file under NDA only. Contact your
local sales office or representative for details.

 

NDA = non-disclosure agreement

 

So, you need to contact a Freescale representative to sign an agreement and then obtain the software.

 

---Tom

0 件の賞賛
返信