I don't find DSP Library mentioned in "Kernel Examples for the StarCore SC3850 DSP Core" document

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I don't find DSP Library mentioned in "Kernel Examples for the StarCore SC3850 DSP Core" document

Jump to solution
2,309 Views
sogico
Contributor I

Hi all,

 

I've been reading the manual "Kernel Examples for the StarCore SC3850 DSP Core" and I'd like to find the examples that are mentioned in this document, about FFT, CRC. It is said in the text that the version which contains all related examples is v10.1.x, but I didn't find that version available online... I use CodeWarrior for StarCore version 10.2.9.

 

Thanks

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,831 Views
J2MEJediMaster
Specialist I

The last paragraph on the opening page of application note AN4207 "Kernel Examples for the StarCore
SC3850 DSP Core", states:

 

NOTE
The supporting software library is available
as a zip file under NDA only. Contact your
local sales office or representative for details.

 

NDA = non-disclosure agreement

 

So, you need to contact a Freescale representative to sign an agreement and then obtain the software.

 

---Tom

View solution in original post

0 Kudos
Reply
1 Reply
1,832 Views
J2MEJediMaster
Specialist I

The last paragraph on the opening page of application note AN4207 "Kernel Examples for the StarCore
SC3850 DSP Core", states:

 

NOTE
The supporting software library is available
as a zip file under NDA only. Contact your
local sales office or representative for details.

 

NDA = non-disclosure agreement

 

So, you need to contact a Freescale representative to sign an agreement and then obtain the software.

 

---Tom

0 Kudos
Reply