Enabling DHCP on MSC8156

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling DHCP on MSC8156

ソリューションへジャンプ
2,654件の閲覧回数
jiboy
Contributor I

Hi,

  Finally i have successfully done the Ethernet as per the demo application in CW.

But is it possible to make the ADS board acquire IP address from the DHCP server. Basically to avoid hard coded IP address usage in the code?

  If there is an example of DHCP on MSC8156, please let me know.

 

I did search the database and found DHCP enabled for some other products but not for StarCORE.

Please advice.

 

Thanks,

Bijoy

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,142件の閲覧回数
Jim95
Contributor III

Hello,

 

Look the tfpt demo, it uses the DHCP to set the board IP adress.

 

Reagards.

 

Jimmy

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,143件の閲覧回数
Jim95
Contributor III

Hello,

 

Look the tfpt demo, it uses the DHCP to set the board IP adress.

 

Reagards.

 

Jimmy

0 件の賞賛
返信
2,142件の閲覧回数
jiboy
Contributor I

Thanks Jimmy. I checked and its good example.

 

-jiboy

0 件の賞賛
返信