Enabling DHCP on MSC8156

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Enabling DHCP on MSC8156

跳至解决方案
2,682 次查看
jiboy
Contributor I

Hi,

  Finally i have successfully done the Ethernet as per the demo application in CW.

But is it possible to make the ADS board acquire IP address from the DHCP server. Basically to avoid hard coded IP address usage in the code?

  If there is an example of DHCP on MSC8156, please let me know.

 

I did search the database and found DHCP enabled for some other products but not for StarCORE.

Please advice.

 

Thanks,

Bijoy

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,170 次查看
Jim95
Contributor III

Hello,

 

Look the tfpt demo, it uses the DHCP to set the board IP adress.

 

Reagards.

 

Jimmy

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,171 次查看
Jim95
Contributor III

Hello,

 

Look the tfpt demo, it uses the DHCP to set the board IP adress.

 

Reagards.

 

Jimmy

0 项奖励
回复
2,170 次查看
jiboy
Contributor I

Thanks Jimmy. I checked and its good example.

 

-jiboy

0 项奖励
回复