Enabling DHCP on MSC8156

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling DHCP on MSC8156

Jump to solution
2,637 Views
jiboy
Contributor I

Hi,

  Finally i have successfully done the Ethernet as per the demo application in CW.

But is it possible to make the ADS board acquire IP address from the DHCP server. Basically to avoid hard coded IP address usage in the code?

  If there is an example of DHCP on MSC8156, please let me know.

 

I did search the database and found DHCP enabled for some other products but not for StarCORE.

Please advice.

 

Thanks,

Bijoy

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,125 Views
Jim95
Contributor III

Hello,

 

Look the tfpt demo, it uses the DHCP to set the board IP adress.

 

Reagards.

 

Jimmy

View solution in original post

0 Kudos
Reply
2 Replies
2,126 Views
Jim95
Contributor III

Hello,

 

Look the tfpt demo, it uses the DHCP to set the board IP adress.

 

Reagards.

 

Jimmy

0 Kudos
Reply
2,125 Views
jiboy
Contributor I

Thanks Jimmy. I checked and its good example.

 

-jiboy

0 Kudos
Reply