Build Error - LLT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Build Error - LLT

跳至解决方案
2,680 次查看
ITCO00
Contributor III

Hello,

 

I'm using CW 10.1.3 for MC8156 SmartDSP.

While building a specific C file (size is ~45Kb) in optimization level 3, I've received the following error:

RA ERROR 2: Temporary spill variable spilled. PROCESS IS TERMINATED

What does it mean?

 

Thanks

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,159 次查看
CrasyCat
Specialist III

Hello

 

Can you give it a try with CodeWarrior for Starcore V10.1.5, which is available from our download page

(http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-STARCORE-DSP10&fpsp=1&tab=Design_T...

 

There were a couple of these "RA ERROR 2: Temporary spill variable spilled" errors fixed in there.

If the issue is still present, please submit a service request at following URL:

    https://www.freescale.com/webapp/servicerequest.create_SR.framework?regFlag=fromOpenSR

 

make sure to attach the preprocessor listing for the source file generating the issue as well as the command line options you are using to build.

 

 

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,160 次查看
CrasyCat
Specialist III

Hello

 

Can you give it a try with CodeWarrior for Starcore V10.1.5, which is available from our download page

(http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-STARCORE-DSP10&fpsp=1&tab=Design_T...

 

There were a couple of these "RA ERROR 2: Temporary spill variable spilled" errors fixed in there.

If the issue is still present, please submit a service request at following URL:

    https://www.freescale.com/webapp/servicerequest.create_SR.framework?regFlag=fromOpenSR

 

make sure to attach the preprocessor listing for the source file generating the issue as well as the command line options you are using to build.

 

 

CrasyCat

0 项奖励
回复