Build Error - LLT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,638件の閲覧回数
ITCO00
Contributor III

Hello,

 

I'm using CW 10.1.3 for MC8156 SmartDSP.

While building a specific C file (size is ~45Kb) in optimization level 3, I've received the following error:

RA ERROR 2: Temporary spill variable spilled. PROCESS IS TERMINATED

What does it mean?

 

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,117件の閲覧回数
CrasyCat
Specialist III

Hello

 

Can you give it a try with CodeWarrior for Starcore V10.1.5, which is available from our download page

(http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-STARCORE-DSP10&fpsp=1&tab=Design_T...

 

There were a couple of these "RA ERROR 2: Temporary spill variable spilled" errors fixed in there.

If the issue is still present, please submit a service request at following URL:

    https://www.freescale.com/webapp/servicerequest.create_SR.framework?regFlag=fromOpenSR

 

make sure to attach the preprocessor listing for the source file generating the issue as well as the command line options you are using to build.

 

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,118件の閲覧回数
CrasyCat
Specialist III

Hello

 

Can you give it a try with CodeWarrior for Starcore V10.1.5, which is available from our download page

(http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-STARCORE-DSP10&fpsp=1&tab=Design_T...

 

There were a couple of these "RA ERROR 2: Temporary spill variable spilled" errors fixed in there.

If the issue is still present, please submit a service request at following URL:

    https://www.freescale.com/webapp/servicerequest.create_SR.framework?regFlag=fromOpenSR

 

make sure to attach the preprocessor listing for the source file generating the issue as well as the command line options you are using to build.

 

 

CrasyCat

0 件の賞賛
返信