how to load the boot code into the nor flash of p2041

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to load the boot code into the nor flash of p2041

跳至解决方案
1,443 次查看
jagxin
Contributor III

hai

         I have completed the por sequence of my board how to load  the boot code to the nor flash through tap controller using code warrior .please provide if any procedure is there in loading the code and how to find the code is loaded successfully into the flash 

标签 (1)
0 项奖励
回复
1 解答
1,171 次查看
marius_grigoras
NXP Employee
NXP Employee

Hi,

Please take a look here [1] - it's basically the same question.

Thank you,

Marius

[1] https://community.freescale.com/message/588062?et=watches.email.thread#588062

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,171 次查看
yinux
Contributor III

I use p2041 rdb, i cannot program the flash using the TAP,  how to do? 

does the codewarrior support the p2041rdb nor flash erase? 

I cannot find the ease xml of p2041rdb nor flash ,  shoud I modify?

0 项奖励
回复
1,171 次查看
jagxin
Contributor III

dear sir

                I have used p2041 sram init .tcl file for initialitation and i was able to connect to the processor but when i am trying to erase the flash NOR flash the following errors are occurring how to solve this what are the possibilities all the schematics i have used the same as of evm except that i have used  this part of flash S29GL01GS10TFI010  instead of GP series

Capturewqeytrte.PNG

i have used the same init file  P2041RDB_init_sram.tcl provided from freescale do i have to change any setting in the init file i have used the S29GL01GP series for the flash device do the erasing algorithm mentioned in the .xml file is same for both flash series how to create a new flash .xml with eml file

regards

AGXIN.J

0 项奖励
回复
1,172 次查看
marius_grigoras
NXP Employee
NXP Employee

Hi,

Please take a look here [1] - it's basically the same question.

Thank you,

Marius

[1] https://community.freescale.com/message/588062?et=watches.email.thread#588062

0 项奖励
回复