Hi,
Please take a look here [1] - it's basically the same question.
Thank you,
Marius
[1] https://community.freescale.com/message/588062?et=watches.email.thread#588062
I use p2041 rdb, i cannot program the flash using the TAP, how to do?
does the codewarrior support the p2041rdb nor flash erase?
I cannot find the ease xml of p2041rdb nor flash , shoud I modify?
dear sir
I have used p2041 sram init .tcl file for initialitation and i was able to connect to the processor but when i am trying to erase the flash NOR flash the following errors are occurring how to solve this what are the possibilities all the schematics i have used the same as of evm except that i have used this part of flash S29GL01GS10TFI010 instead of GP series
i have used the same init file P2041RDB_init_sram.tcl provided from freescale do i have to change any setting in the init file i have used the S29GL01GP series for the flash device do the erasing algorithm mentioned in the .xml file is same for both flash series how to create a new flash .xml with eml file
regards
AGXIN.J
Hi,
Please take a look here [1] - it's basically the same question.
Thank you,
Marius
[1] https://community.freescale.com/message/588062?et=watches.email.thread#588062