how to load the boot code into the nor flash of p2041

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to load the boot code into the nor flash of p2041

Jump to solution
1,434 Views
jagxin
Contributor III

hai

         I have completed the por sequence of my board how to load  the boot code to the nor flash through tap controller using code warrior .please provide if any procedure is there in loading the code and how to find the code is loaded successfully into the flash 

Labels (1)
0 Kudos
Reply
1 Solution
1,162 Views
marius_grigoras
NXP Employee
NXP Employee

Hi,

Please take a look here [1] - it's basically the same question.

Thank you,

Marius

[1] https://community.freescale.com/message/588062?et=watches.email.thread#588062

View solution in original post

0 Kudos
Reply
3 Replies
1,162 Views
yinux
Contributor III

I use p2041 rdb, i cannot program the flash using the TAP,  how to do? 

does the codewarrior support the p2041rdb nor flash erase? 

I cannot find the ease xml of p2041rdb nor flash ,  shoud I modify?

0 Kudos
Reply
1,162 Views
jagxin
Contributor III

dear sir

                I have used p2041 sram init .tcl file for initialitation and i was able to connect to the processor but when i am trying to erase the flash NOR flash the following errors are occurring how to solve this what are the possibilities all the schematics i have used the same as of evm except that i have used  this part of flash S29GL01GS10TFI010  instead of GP series

Capturewqeytrte.PNG

i have used the same init file  P2041RDB_init_sram.tcl provided from freescale do i have to change any setting in the init file i have used the S29GL01GP series for the flash device do the erasing algorithm mentioned in the .xml file is same for both flash series how to create a new flash .xml with eml file

regards

AGXIN.J

0 Kudos
Reply
1,163 Views
marius_grigoras
NXP Employee
NXP Employee

Hi,

Please take a look here [1] - it's basically the same question.

Thank you,

Marius

[1] https://community.freescale.com/message/588062?et=watches.email.thread#588062

0 Kudos
Reply