error:Stepping using step range is taking too long,resuming process.  what is problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

error:Stepping using step range is taking too long,resuming process.  what is problem

2,313 次查看
sunwind45
Contributor I
CodeWarrior for PPC:smileyfrustrated:tepping using step range is taking too long,resuming process.
 
give me a idea about it!
 
thanks
标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,096 次查看
Black
Contributor I

If you step over a function and the target doesn't stop (the CodeWarrior Debugger cannot read the PC) then this error is returned. A CodeWarrior CCS log could help tracking down this issue (in Project Settings, Remote Debugging panel, select Edit Connection and check Enable Logging).

I hope this helps.

0 项奖励
回复

1,096 次查看
sunwind45
Contributor I
Thanks for your idea.
I'll  try it. 
 
Otherwise,
This error is returned when loading the object file into mpc862 using PowerTAP Emulator.
 
Is the hardware bad? Or mpc862 is bad? Or BDM on mpc862 is bad?
0 项奖励
回复