error:Stepping using step range is taking too long,resuming process.  what is problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error:Stepping using step range is taking too long,resuming process.  what is problem

2,901 Views
sunwind45
Contributor I
CodeWarrior for PPC:smileyfrustrated:tepping using step range is taking too long,resuming process.
 
give me a idea about it!
 
thanks
Labels (1)
0 Kudos
Reply
2 Replies

1,684 Views
Black
Contributor I

If you step over a function and the target doesn't stop (the CodeWarrior Debugger cannot read the PC) then this error is returned. A CodeWarrior CCS log could help tracking down this issue (in Project Settings, Remote Debugging panel, select Edit Connection and check Enable Logging).

I hope this helps.

0 Kudos
Reply

1,684 Views
sunwind45
Contributor I
Thanks for your idea.
I'll  try it. 
 
Otherwise,
This error is returned when loading the object file into mpc862 using PowerTAP Emulator.
 
Is the hardware bad? Or mpc862 is bad? Or BDM on mpc862 is bad?
0 Kudos
Reply