Target processor setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Target processor setting

Jump to solution
2,539 Views
Chanh
Contributor III

Hi,

I am using CodeWarrior for QorIQ LS Series with FRWY-LS1046A board, I follow the user manual to create bare metal project. When I go the the setting page, the target processor is cortex-m3 and cannot be changed. May I know any problem with that option if I run the binary file on the board? And how to change the processor to cortex-a72?

Thanks.

0 Kudos
Reply
1 Solution
2,534 Views
yipingwang
NXP TechSupport
NXP TechSupport

No need to do modification, please use the default setting, this option will not be used in the compilation.

View solution in original post

0 Kudos
Reply
2 Replies
2,523 Views
Chanh
Contributor III

Hi Yiping,

Got it. Thanks.

0 Kudos
Reply
2,535 Views
yipingwang
NXP TechSupport
NXP TechSupport

No need to do modification, please use the default setting, this option will not be used in the compilation.

0 Kudos
Reply