Hi,
I have accidentally erased the code from NAND flash while booting from NOR flash. Now my board is not booting up.
Does any one knows the steps to flash u-boot NOR binary files to NOR flash.
For your information I am using P1010RDB-PB. Switch settings are correct as mentioned in the documents.
已解决! 转到解答。
Hi Yiping Wang,
When I tried "source IDcode.tcl" I am able to see the USB tap being connected in CCS.
Which means the usbtap is working and properly configured and detected by CodeWarrior IDE.
I need to boot the P1010RDB-PB board from NOR flash. So I configured the switch settings in such a way that it boot from NOR flash if proper code is available in it (starting address of physical memory map of NOR flash). In order for the code to be available the binaries need to be written into the flash.
I am using CodeWarrior for PA 10.4.0. and init files as P1010RDB-PB_init_core.tcl. Corresponding u-boot.bin file is selected in Add program (action chosen for the target task).
I am not sure what step I missed
Thanks
Nobel
One way is to use Flash Programmer from CodeWarrior for PA. Take a look on Targeting Manual and AN4948 for more information.
Adrian
Hi Adrian,
Thanks, I tried the same but got some error message.
Error: The algorithm was not able to run on the target or the flash is not configured properly.
Error: Getting flash ID failed
Error: The algorithm was not able to run on the target or the flash is not configured properly.
hi Adrian,
create a codewarrior bareboard project
processor -> QorIQ_P1 -> P1010
Debug target settings
Board: P1010RDB-PB
Launch: Download SRAM
Connection type: USB TAP
Then I follow the steps mention in AN4948.pdf, instead of NAND I choose NOR
and the switch settings as mentioned in P1010RDB_Board_Bringup.pdf.
While following the steps green execute button is greyed. So I change the run configuration.
After that execute button appear. When executed I got the below log.
fl::target -lc "p1010_boot_test-core00_SRAM_P1010_Download"
fl::target -b 0x0 0x40000
fl::target -v off -l off
cmdwin::fl::device -d "S29GL256P" -o "16Mx16x1" -a 0xfe000000 0xffffffff
cmdwin::fl::image -f "/home/inno/Nobel/project/P1010RDB/Source/yocto/QorIQ-SDK-V1.8-20150619-yocto/build_p1010rdb_release/tmp/work/p1010rdb-fsl-linux-gnuspe/u-boot-qoriq/2014.07+fslgit-r0/git/P1010RDB-PB_NOR/u-boot.bin" -t "Auto Detect" -re off -oe on -o 0xfe000000
cmdwin::fl::erase image
Beginning Operation ...
-------------------------
Auto-detection is successful.
File is of type Binary/Raw Format.
Performing target initialization ...
Error: Connect Failed.
Could not connect to the probe (or other debug link)
[CCS last error: CC config string is invalid ](CCSProtocolPlugin)
Error: Connect Failed.
This is a connection issue. Check, as Yiping already suggested, if ccs drivers are installed. Also, you can check directly in ccs (/usr/local/Freescale/CodeWarrior_PA_10.5.0/PA/ccs/bin and run ../ccs) if utap probe is found (in ccs console run this command: findcc utaps).
Adrian
 yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Nobel,
According to your description, it seems that you are using Linux OS, you need to install CCS USB driver manually. Please follow /usr/local/Freescale/CodeWarrior_PA_10.5.0/PA/ccs/drivers/usb/readme.usbtap.txt
to create new udev rules and make them take effect. If you use CodeWarrior TAP with USB connection please refer to readme.cwtap.txt.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yiping Wang,
When I tried "source IDcode.tcl" I am able to see the USB tap being connected in CCS.
Which means the usbtap is working and properly configured and detected by CodeWarrior IDE.
I need to boot the P1010RDB-PB board from NOR flash. So I configured the switch settings in such a way that it boot from NOR flash if proper code is available in it (starting address of physical memory map of NOR flash). In order for the code to be available the binaries need to be written into the flash.
I am using CodeWarrior for PA 10.4.0. and init files as P1010RDB-PB_init_core.tcl. Corresponding u-boot.bin file is selected in Add program (action chosen for the target task).
I am not sure what step I missed
Thanks
Nobel
 yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Nobel,
Please check whether the CodeWarrior license is still valid from Help->Freescale Licenses in CodeWarrior IDE.
In addition, would you please provide the log of the command "source IDcode.tcl".
Thanks,
Yiping
Hi Yiping,
Please find the log below,
CodeWarrior Connection Server console display active (Tcl8.4.6 / Tk8.4.6)
Loading CCSAPI Tcl interface (/opt/Freescale/PA/ccs/bin/ccstcl.so)...
Loading Svfburner (/opt/Freescale/PA/ccs/bin/svfburner.so)...
Server listening on port: 41475
Clients allowed from all hosts
No clients denied
(bin) 7 % findcc utaps
USB TAP Serial Numbers:
12022278
12022278
(bin) 8 % source IDcode.tcl
canning for available TAPs connected via USB.....
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
+
+ Available Remote Connections
+
+ 1 - USBTAP - 12022278
+ 2 - CodeWarriorTAP - <Specify IP Address>
+ 3 - EthernetTAP - <Specify IP Address>
+ 4 - GigabitTAP - <Specify IP Address>
+
+ x - Exit Script without Changes
+
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
Specify connection:
1
Configuring TAP Interface....
Configured Connection: utap : 12022278
USB receive reply failure
(bin) 9 %
(bin) 15 % show cc
0: USB TAP (JTAG) (utap:12022278) Loader software ver. {1.10}
Sending code to USB TAP - please wait
0: USB TAP (JTAG) (utap:12022278) CC software ver. {1.3}
(bin) 15 % scanboard
TDO -----
|
* Device 0 IDCODE: 1692301D Device: FSL P1010 rev 2.x
|
TDI -----
 yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Nobel,
It is a little weird, according to the CCS console information, the CCS driver works normally, but CodeWarrior IDE reports CCS failed to connect to USB TAP. (Please make sure CodeWarrior license doesn't expire).
Would you please use the following procedure to capture CCS log in CodeWarrior IDE and send it to me? It contains detailed communication information between CodeWarrior and the target board.
Please enable CCS log from "Run->Debug Configurations -><project>-core0_RAM_-Connect(Download)->Edit...->Advanced->Advanced CCS setting->Enable logging", and connect to the target from "Run->Debug Configurations-><project>-core0_RAM_-Connect(Download)->Debug”, the CCS log will be displayed in the console panel in CodeWarrior IDE.
Note:
If the CCS log in the console is truncated, please enlarge the console buffer from Window->Preferences->Run/Debug->Console->uncheck "Limit console output". (Please open the console panel from Window->Show View->Console, and if nothing displayed, please choose the correct session on the right top icon.)
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yiping,
Kindly see the log below,
ccs_open
ipaddr = 127.0.0.1
port = 41475
timeout = 15
serverh = 0
ccs_open; ccs_error = 10
Error message: Connection refused
ccs_open
ipaddr = 127.0.0.1
port = 41475
timeout = 15
serverh = 0
ccs_open; ccs_error = 10
Error message: Connection refused
ccs_open
ipaddr = 127.0.0.1
port = 41475
timeout = 15
serverh = 0
ccs_open; ccs_error = 10
Error message: Connection refused
ccs_open
ipaddr = 127.0.0.1
port = 41475
timeout = 15
serverh = 0
ccs_open; ccs_error = 10
Error message: Connection refused
ccs_open
ipaddr = 127.0.0.1
port = 41475
timeout = 15
serverh = 0
ccs_open; ccs_error = 0
ccs_get_connection_count
serverh = 0
count = 1
ccs_get_connection_count; ccs_error = 0
ccs_available_connections
serverh = 0
count = 0
ccs_available_connections; ccs_error = 0
ccs_available_connections
serverh = 0
count = 0
ccs_available_connections; ccs_error = 0
ccs_config_cc
serverh = 0
config_string = utap:0
ccs_config_cc; ccs_error = 0
ccs_available_connections
serverh = 0
count = 0
ccs_available_connections; ccs_error = 2
Error message: Network timeout
ccs_kill_server
serverh = 0
ccs_kill_server; ccs_error = 14
Error message: Invalid sequence number
FYI, it was working previously then it stop working can't able to flash it.(Now I am using Custom Board).
Let me know If I need to start a new thread to discuss. and I am using Linux environment.
 yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Noble,
The CCS connection problem is caused by CodeWarrior IDE configuration or CodeWarrior itself, it is not related with the target board or USB TAP.
Please open the panel "Hardware or Simulator Connection" from Run->Debug Configurations -><project>-core0_RAM_-Connect(Download)->Edit->Connection, please make sure CCS server is configured as "Automatic launch” rather than "Manual launch".
If this problem remains, I suggest you create a bare board project in a new workspace following new project wizards.
You could create a new thread if needed.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------