S-Record file generation. Codewarrior v7.1 using m52259DEMOMCU.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S-Record file generation. Codewarrior v7.1 using m52259DEMOMCU.

ソリューションへジャンプ
1,439件の閲覧回数
Zaas
Contributor I

Dear all,

 

I have a doubt related S-Record file generation.
I'm correct if I assume that with v2 colfire having contiguous sectors flash always the output S-record file generated will have adjacent address flash where the data will be loaded.
What I mean that the S-record file generated is linear asigned. The address is not jumping within flash from one to another address.


Thanks in advanced.
   

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
738件の閲覧回数
CrasyCat
Specialist III

Hello

 

Yes S record file should contain records with adjacent address.  

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
739件の閲覧回数
CrasyCat
Specialist III

Hello

 

Yes S record file should contain records with adjacent address.  

 

CrasyCat

0 件の賞賛
返信