S-Record file generation. Codewarrior v7.1 using m52259DEMOMCU.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S-Record file generation. Codewarrior v7.1 using m52259DEMOMCU.

跳至解决方案
1,750 次查看
Zaas
Contributor I

Dear all,

 

I have a doubt related S-Record file generation.
I'm correct if I assume that with v2 colfire having contiguous sectors flash always the output S-record file generated will have adjacent address flash where the data will be loaded.
What I mean that the S-record file generated is linear asigned. The address is not jumping within flash from one to another address.


Thanks in advanced.
   

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,049 次查看
CrasyCat
Specialist III

Hello

 

Yes S record file should contain records with adjacent address.  

 

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,050 次查看
CrasyCat
Specialist III

Hello

 

Yes S record file should contain records with adjacent address.  

 

CrasyCat

0 项奖励
回复