S-Record file generation. Codewarrior v7.1 using m52259DEMOMCU.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S-Record file generation. Codewarrior v7.1 using m52259DEMOMCU.

Jump to solution
1,760 Views
Zaas
Contributor I

Dear all,

 

I have a doubt related S-Record file generation.
I'm correct if I assume that with v2 colfire having contiguous sectors flash always the output S-record file generated will have adjacent address flash where the data will be loaded.
What I mean that the S-record file generated is linear asigned. The address is not jumping within flash from one to another address.


Thanks in advanced.
   

Labels (1)
0 Kudos
Reply
1 Solution
1,059 Views
CrasyCat
Specialist III

Hello

 

Yes S record file should contain records with adjacent address.  

 

CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
1,060 Views
CrasyCat
Specialist III

Hello

 

Yes S record file should contain records with adjacent address.  

 

CrasyCat

0 Kudos
Reply