Request for m29EW flash xml patch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Request for m29EW flash xml patch

1,197件の閲覧回数
anqiren-b47842
NXP Employee
NXP Employee

Hi, customer ASB are using CodeWarrior 10.4 for flashing uboot on P4080 board, while their flash type is M29EW, which CW doesn't support by default. Could you pls offer me one patch for this flash type? Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

967件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Anqi Ren,

The latest version CodeWarrior doesn't support M29EW in the device list either.

Please try to use the one flash programming algorithm for AMD in C:\Freescale\CW_PA_v10.5.0\PA\bin\plugins\support\Flash_Programmer\EPPC according to your flash organization, probably you may choose amd16x2.elf.

Please refer to C:\Freescale\CW_PA_v10.5.0\PA\bin\plugins\support\Products\ProductData\FPDevices.mwpdb\FP\M29DW128G.xml and C:\Freescale\CW_PA_v10.5.0\PA\bin\plugins\support\Products\ProductData\FPDevices.mwpdb\product-manifest.xm to add device M29EW in CodeWarrior IDE by yourself.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信