Manufacturing boards with LS1012A processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Manufacturing boards with LS1012A processor

Jump to solution
2,134 Views
zmlopez
Contributor III

I'm thinking about a new project of a board with LS1012A processor.

I've got a doubt about how to write the nor flash in new boards in manufacturing process.

It seems that the only way to flash spi nor memory in new boards is with Codewarrior TAP through JTAG, because it doesn't have any USB/Ethernet/serial booth method inside its ROM, only SPI nor flash.

Is there other available method to program spi nor in new boards besides Codewarrior TAP, more adecuate to manufacturing processes?

Thanks in advance.

Labels (1)
0 Kudos
Reply
1 Solution
1,739 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello miguel lopez,

Please download and install CodeWarrior for ARMv8 from CodeWarrior Dev Tools for Networked Apps|NXP .

Please refer to the procedure described in https://community.nxp.com/thread/439034?commentID=852508#comment-852508  to program RCW and u-boot to QSPI flash.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,740 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello miguel lopez,

Please download and install CodeWarrior for ARMv8 from CodeWarrior Dev Tools for Networked Apps|NXP .

Please refer to the procedure described in https://community.nxp.com/thread/439034?commentID=852508#comment-852508  to program RCW and u-boot to QSPI flash.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply