Manufacturing boards with LS1012A processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Manufacturing boards with LS1012A processor

ソリューションへジャンプ
2,179件の閲覧回数
zmlopez
Contributor III

I'm thinking about a new project of a board with LS1012A processor.

I've got a doubt about how to write the nor flash in new boards in manufacturing process.

It seems that the only way to flash spi nor memory in new boards is with Codewarrior TAP through JTAG, because it doesn't have any USB/Ethernet/serial booth method inside its ROM, only SPI nor flash.

Is there other available method to program spi nor in new boards besides Codewarrior TAP, more adecuate to manufacturing processes?

Thanks in advance.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,784件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello miguel lopez,

Please download and install CodeWarrior for ARMv8 from CodeWarrior Dev Tools for Networked Apps|NXP .

Please refer to the procedure described in https://community.nxp.com/thread/439034?commentID=852508#comment-852508  to program RCW and u-boot to QSPI flash.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,785件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello miguel lopez,

Please download and install CodeWarrior for ARMv8 from CodeWarrior Dev Tools for Networked Apps|NXP .

Please refer to the procedure described in https://community.nxp.com/thread/439034?commentID=852508#comment-852508  to program RCW and u-boot to QSPI flash.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信