MCF51JM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
2,687 Views
sethpoly
Contributor II

Codewarrior 6.1 service pack

 

Why is the MCF51JM family not supported?

The MCF51QE is the only family listed when starting a new project.

Labels (1)
0 Kudos
Reply
1 Solution
1,573 Views
sethpoly
Contributor II

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061788213CF333D

 

 

This service pack includes support for the MCF51JM128 and MCF51JM64 derivatives in the form of:

• UNIS Processor Expert support
• Flash programming and debug support
• Derivative-specific C header, source and PRM files
• Derivative-specific assembly include file
• P&E target connection drivers
• SofTec Microsystems inDart HCS08 BDM support
• Open Source BDM connection support

This service pack also increases the RAM size of the JM64 from 8K to 16K

Note: For full Processor Expert functionality the latest Processor Expert service pack, obtainable from the same source as this service pack, must also be installed.

View solution in original post

0 Kudos
Reply
1 Reply
1,574 Views
sethpoly
Contributor II

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061788213CF333D

 

 

This service pack includes support for the MCF51JM128 and MCF51JM64 derivatives in the form of:

• UNIS Processor Expert support
• Flash programming and debug support
• Derivative-specific C header, source and PRM files
• Derivative-specific assembly include file
• P&E target connection drivers
• SofTec Microsystems inDart HCS08 BDM support
• Open Source BDM connection support

This service pack also increases the RAM size of the JM64 from 8K to 16K

Note: For full Processor Expert functionality the latest Processor Expert service pack, obtainable from the same source as this service pack, must also be installed.

0 Kudos
Reply