MCF51JM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
2,666 次查看
sethpoly
Contributor II

Codewarrior 6.1 service pack

 

Why is the MCF51JM family not supported?

The MCF51QE is the only family listed when starting a new project.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,552 次查看
sethpoly
Contributor II

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061788213CF333D

 

 

This service pack includes support for the MCF51JM128 and MCF51JM64 derivatives in the form of:

• UNIS Processor Expert support
• Flash programming and debug support
• Derivative-specific C header, source and PRM files
• Derivative-specific assembly include file
• P&E target connection drivers
• SofTec Microsystems inDart HCS08 BDM support
• Open Source BDM connection support

This service pack also increases the RAM size of the JM64 from 8K to 16K

Note: For full Processor Expert functionality the latest Processor Expert service pack, obtainable from the same source as this service pack, must also be installed.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,553 次查看
sethpoly
Contributor II

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061788213CF333D

 

 

This service pack includes support for the MCF51JM128 and MCF51JM64 derivatives in the form of:

• UNIS Processor Expert support
• Flash programming and debug support
• Derivative-specific C header, source and PRM files
• Derivative-specific assembly include file
• P&E target connection drivers
• SofTec Microsystems inDart HCS08 BDM support
• Open Source BDM connection support

This service pack also increases the RAM size of the JM64 from 8K to 16K

Note: For full Processor Expert functionality the latest Processor Expert service pack, obtainable from the same source as this service pack, must also be installed.

0 项奖励
回复