MCF51JM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,664件の閲覧回数
sethpoly
Contributor II

Codewarrior 6.1 service pack

 

Why is the MCF51JM family not supported?

The MCF51QE is the only family listed when starting a new project.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,550件の閲覧回数
sethpoly
Contributor II

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061788213CF333D

 

 

This service pack includes support for the MCF51JM128 and MCF51JM64 derivatives in the form of:

• UNIS Processor Expert support
• Flash programming and debug support
• Derivative-specific C header, source and PRM files
• Derivative-specific assembly include file
• P&E target connection drivers
• SofTec Microsystems inDart HCS08 BDM support
• Open Source BDM connection support

This service pack also increases the RAM size of the JM64 from 8K to 16K

Note: For full Processor Expert functionality the latest Processor Expert service pack, obtainable from the same source as this service pack, must also be installed.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,551件の閲覧回数
sethpoly
Contributor II

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061788213CF333D

 

 

This service pack includes support for the MCF51JM128 and MCF51JM64 derivatives in the form of:

• UNIS Processor Expert support
• Flash programming and debug support
• Derivative-specific C header, source and PRM files
• Derivative-specific assembly include file
• P&E target connection drivers
• SofTec Microsystems inDart HCS08 BDM support
• Open Source BDM connection support

This service pack also increases the RAM size of the JM64 from 8K to 16K

Note: For full Processor Expert functionality the latest Processor Expert service pack, obtainable from the same source as this service pack, must also be installed.

0 件の賞賛
返信