M52235EVB  internal ROM Target application, P&E Coldfire MULTILINK debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M52235EVB  internal ROM Target application, P&E Coldfire MULTILINK debugger

1,892 Views
internike
Contributor I
Anyone has tryed to debug the application, uploading object code into INTERNAL FLASH? Is there any possibility to load object code without using FlashProgrammer: that is load object code at DEBUG command? Luigi.
Labels (1)
0 Kudos
Reply
1 Reply

980 Views
vpmeister
Contributor I
I need the same thing. I can download the program to ROM with the programmer, and debug it if I download to RAM, but have not figured out how to debug in ROM yet.
0 Kudos
Reply