Coldfire: Obtaining details about the build process

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Coldfire: Obtaining details about the build process

3,479 Views
mjbcswitzerland
Specialist V

Hi all

 

I am using CW 6.3 for the Coldfire and have noted the following.
When the project is built there are windows which appear very briefly with some information about the compile and link steps but at the end - assuming no errors - everything disappears.

 

How is it possible to see what actually happened? Can the data which appears briefely in these windows be viewed later in a log file or something?

 

The reason is to be able to check on some details - paths used, flags used etc. The goal is to check the build process in the CW IDE environment with a command line build process. Presently this has not proved to be possible but I assume that the info is hanging around someweher (or can be activated) but the question is where and how???

 

Thanks for any help

 

Regards

 

Mark Butcher
www.mjbc.ch / www.uTasker.com

Message Edited by CrasyCat on 2007-04-13 01:44 PM

Labels (1)
0 Kudos
Reply
3 Replies

1,507 Views
Alban
Senior Contributor II
Hi Mark,
 
Have you looked at CrazyCat suggestion: Code Warior Errors and Warnings
 
Alban.
0 Kudos
Reply

1,507 Views
mjbcswitzerland
Specialist V
Hi Alban

Using the "Touch" method there is quite a lot of detail. I hope that the relevant info can be found there. I'm trying to help a uTasker user who wants to convert to command line compiling and has a linker problem that way. I don't know exactly which info he is looking for but hope it can be find now. Possibly it will solve his issue for him - if not I will ask him to post more details here.

Regards

Mark
0 Kudos
Reply

1,507 Views
Alban
Senior Contributor II
Mark,
 
If he's using the command line and things are displayed on the screen, he could use sceeen redirection to a file.
 
Alban.
0 Kudos
Reply