M52235EVB  internal ROM Target application, P&E Coldfire MULTILINK debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M52235EVB  internal ROM Target application, P&E Coldfire MULTILINK debugger

1,874件の閲覧回数
internike
Contributor I
Anyone has tryed to debug the application, uploading object code into INTERNAL FLASH? Is there any possibility to load object code without using FlashProgrammer: that is load object code at DEBUG command? Luigi.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

962件の閲覧回数
vpmeister
Contributor I
I need the same thing. I can download the program to ROM with the programmer, and debug it if I download to RAM, but have not figured out how to debug in ROM yet.
0 件の賞賛
返信