How to capture the Console in debugging a JTAG configuration issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to capture the Console in debugging a JTAG configuration issue

Jump to solution
4,117 Views
kbell_hardware
Contributor III

I'm trying to debug an issue where "CCSProtocolPlugin : Failed to correctly configure the JTAG chain" even though i've run the CCS IDcode.tcl and ir commands in the server and the chain looks fine. My JTAG chain text file matches the CW JTAG file format, i've even used the processor expert to output the file i need and it still doesn't work. I've enabled logging so i can catch where it fails in the console output but the console deletes everything automatically when it fails. I changed the settings so the console would output to a file but the file is always blank. How can i capture the log? I've tried selecting all and copying as fast as i can and what i get is pasted below. I'm trying to connect to a T2080 with the CodeWarrior TAP over USB.

 

I've done this multiple times, it appears to be normal that the connection is refused one or two times at first before it continues. It writes all of the RCW registers and appears to fail when resetting.....or at least that's what i could capture.

 

ccs_open

    ipaddr = 127.0.0.1

    port = 41475

    timeout = 15

    serverh = 0

    ccs_open; ccs_error = 10

    Error message: Connection refused

ccs_open

    ipaddr = 127.0.0.1

    port = 41475

    timeout = 15

    serverh = 0

    ccs_open; ccs_error = 10

    Error message: Connection refused

ccs_open

    ipaddr = 127.0.0.1

    port = 41475

    timeout = 15

    serverh = 0

    ccs_open; ccs_error = 0

ccs_get_connection_count

    serverh = 0

    count = 1

    ccs_get_connection_count; ccs_error = 0

ccs_available_connections

    serverh = 0

    count = 0

    ccs_available_connections; ccs_error = 0

ccs_available_connections

    serverh = 0

    count = 0

    ccs_available_connections; ccs_error = 0

ccs_config_cc

    serverh = 0

    config_string = cwtap:0

    ccs_config_cc; ccs_error = 0

ccs_available_connections

    serverh = 0

    count = 1

    ccs_available_connections; ccs_error = 0

ccs_cc_version

    serverh = 0

    cc = 0

    version.major = 0

    version.minor = 0

    ccs_cc_version; ccs_error = 0

ccs_set_timeout

    serverh = 0

    timeout = 15

    ccs_set_timeout; ccs_error = 0

ccs_available_connections

    serverh = 0

    count = 1

    ccs_available_connections; ccs_error = 0

ccs_config_server

    serverh = 0

    cc = 0

    server_config = 0

    value = 10230

    ccs_config_server; ccs_error = 0

ccs_get_config_chain

    serverh = 0

    device_list: (size = 0)

    ccs_get_config_chain; ccs_error = 0

ccs_config_chain

    serverh = 0

    cc = 0

    device_list: (size = 1)

        device[0]:: core_type=T2080(242)

    ccs_config_chain; ccs_error = 0

ccs_config_template

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    config_reg = 0

    config_data = 500

    ccs_config_template; ccs_error = 0

ccs_config_template

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    config_reg = 2

    config_data = 1

    ccs_config_template; ccs_error = 0

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210001

    count = 1

    size = 4

    value: (size = 4)

         0C00100F

    ccs_write_register; ccs_error = 0; duration=0 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210002

    count = 1

    size = 4

    value: (size = 4)

         05000000

    ccs_write_register; ccs_error = 0; duration=0 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210003

    count = 1

    size = 4

    value: (size = 4)

         00000000

    ccs_write_register; ccs_error = 0; duration=16 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210004

    count = 1

    size = 4

    value: (size = 4)

         00000000

    ccs_write_register; ccs_error = 0; duration=0 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210005

    count = 1

    size = 4

    value: (size = 4)

         6C2D0002

    ccs_write_register; ccs_error = 0; duration=0 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210006

    count = 1

    size = 4

    value: (size = 4)

         F0006A00

    ccs_write_register; ccs_error = 0; duration=0 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210007

    count = 1

    size = 4

    value: (size = 4)

         EC026000

    ccs_write_register; ccs_error = 0; duration=0 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210008

    count = 1

    size = 4

    value: (size = 4)

         C1000000

    ccs_write_register; ccs_error = 0; duration=0 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210009

    count = 1

    size = 4

    value: (size = 4)

         02180000

    ccs_write_register; ccs_error = 0; duration=0 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210010

    count = 1

    size = 4

    value: (size = 4)

         00000001

    ccs_write_register; ccs_error = 0; duration=0 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210011

    count = 1

    size = 4

    value: (size = 4)

         00000000

    ccs_write_register; ccs_error = 0; duration=15 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210012

    count = 1

    size = 4

    value: (size = 4)

         000197FC

    ccs_write_register; ccs_error = 0; duration=2 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210013

    count = 1

    size = 4

    value: (size = 4)

         00000100

    ccs_write_register; ccs_error = 0; duration=2 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210014

    count = 1

    size = 4

    value: (size = 4)

         5280000D

    ccs_write_register; ccs_error = 0; duration=2 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210015

    count = 1

    size = 4

    value: (size = 4)

         00000000

    ccs_write_register; ccs_error = 0; duration=2 ms

ccs_write_register

    coreh = [serverh:0;cc_index:0;chain_pos:0]

    index = 210016

    count = 1

    size = 4

    value: (size = 4)

         00000004

    ccs_write_register; ccs_error = 0; duration=2 ms

ccs_reset_to_debug

    serverh = 0

    cc = 0

Labels (1)
0 Kudos
Reply
1 Solution
3,778 Views
kbell_hardware
Contributor III

I'm new to this environment so i didn't realize that their are multiple console screens and you have to switch back to your logging console to see it.

View solution in original post

0 Kudos
Reply
2 Replies
3,779 Views
kbell_hardware
Contributor III

I'm new to this environment so i didn't realize that their are multiple console screens and you have to switch back to your logging console to see it.

0 Kudos
Reply
3,778 Views
lunminliang
NXP Employee
NXP Employee

Hi,

I think when you remove the termination, the log will show again on the console. No?

Regards

Lunmin

0 Kudos
Reply