I'm trying to debug an issue where "CCSProtocolPlugin : Failed to correctly configure the JTAG chain" even though i've run the CCS IDcode.tcl and ir commands in the server and the chain looks fine. My JTAG chain text file matches the CW JTAG file format, i've even used the processor expert to output the file i need and it still doesn't work. I've enabled logging so i can catch where it fails in the console output but the console deletes everything automatically when it fails. I changed the settings so the console would output to a file but the file is always blank. How can i capture the log? I've tried selecting all and copying as fast as i can and what i get is pasted below. I'm trying to connect to a T2080 with the CodeWarrior TAP over USB.
I've done this multiple times, it appears to be normal that the connection is refused one or two times at first before it continues. It writes all of the RCW registers and appears to fail when resetting.....or at least that's what i could capture.
ccs_open
ipaddr = 127.0.0.1
port = 41475
timeout = 15
serverh = 0
ccs_open; ccs_error = 10
Error message: Connection refused
ccs_open
ipaddr = 127.0.0.1
port = 41475
timeout = 15
serverh = 0
ccs_open; ccs_error = 10
Error message: Connection refused
ccs_open
ipaddr = 127.0.0.1
port = 41475
timeout = 15
serverh = 0
ccs_open; ccs_error = 0
ccs_get_connection_count
serverh = 0
count = 1
ccs_get_connection_count; ccs_error = 0
ccs_available_connections
serverh = 0
count = 0
ccs_available_connections; ccs_error = 0
ccs_available_connections
serverh = 0
count = 0
ccs_available_connections; ccs_error = 0
ccs_config_cc
serverh = 0
config_string = cwtap:0
ccs_config_cc; ccs_error = 0
ccs_available_connections
serverh = 0
count = 1
ccs_available_connections; ccs_error = 0
ccs_cc_version
serverh = 0
cc = 0
version.major = 0
version.minor = 0
ccs_cc_version; ccs_error = 0
ccs_set_timeout
serverh = 0
timeout = 15
ccs_set_timeout; ccs_error = 0
ccs_available_connections
serverh = 0
count = 1
ccs_available_connections; ccs_error = 0
ccs_config_server
serverh = 0
cc = 0
server_config = 0
value = 10230
ccs_config_server; ccs_error = 0
ccs_get_config_chain
serverh = 0
device_list: (size = 0)
ccs_get_config_chain; ccs_error = 0
ccs_config_chain
serverh = 0
cc = 0
device_list: (size = 1)
device[0]:: core_type=T2080(242)
ccs_config_chain; ccs_error = 0
ccs_config_template
coreh = [serverh:0;cc_index:0;chain_pos:0]
config_reg = 0
config_data = 500
ccs_config_template; ccs_error = 0
ccs_config_template
coreh = [serverh:0;cc_index:0;chain_pos:0]
config_reg = 2
config_data = 1
ccs_config_template; ccs_error = 0
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210001
count = 1
size = 4
value: (size = 4)
0C00100F
ccs_write_register; ccs_error = 0; duration=0 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210002
count = 1
size = 4
value: (size = 4)
05000000
ccs_write_register; ccs_error = 0; duration=0 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210003
count = 1
size = 4
value: (size = 4)
00000000
ccs_write_register; ccs_error = 0; duration=16 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210004
count = 1
size = 4
value: (size = 4)
00000000
ccs_write_register; ccs_error = 0; duration=0 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210005
count = 1
size = 4
value: (size = 4)
6C2D0002
ccs_write_register; ccs_error = 0; duration=0 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210006
count = 1
size = 4
value: (size = 4)
F0006A00
ccs_write_register; ccs_error = 0; duration=0 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210007
count = 1
size = 4
value: (size = 4)
EC026000
ccs_write_register; ccs_error = 0; duration=0 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210008
count = 1
size = 4
value: (size = 4)
C1000000
ccs_write_register; ccs_error = 0; duration=0 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210009
count = 1
size = 4
value: (size = 4)
02180000
ccs_write_register; ccs_error = 0; duration=0 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210010
count = 1
size = 4
value: (size = 4)
00000001
ccs_write_register; ccs_error = 0; duration=0 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210011
count = 1
size = 4
value: (size = 4)
00000000
ccs_write_register; ccs_error = 0; duration=15 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210012
count = 1
size = 4
value: (size = 4)
000197FC
ccs_write_register; ccs_error = 0; duration=2 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210013
count = 1
size = 4
value: (size = 4)
00000100
ccs_write_register; ccs_error = 0; duration=2 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210014
count = 1
size = 4
value: (size = 4)
5280000D
ccs_write_register; ccs_error = 0; duration=2 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210015
count = 1
size = 4
value: (size = 4)
00000000
ccs_write_register; ccs_error = 0; duration=2 ms
ccs_write_register
coreh = [serverh:0;cc_index:0;chain_pos:0]
index = 210016
count = 1
size = 4
value: (size = 4)
00000004
ccs_write_register; ccs_error = 0; duration=2 ms
ccs_reset_to_debug
serverh = 0
cc = 0
解決済! 解決策の投稿を見る。
I'm new to this environment so i didn't realize that their are multiple console screens and you have to switch back to your logging console to see it.
I'm new to this environment so i didn't realize that their are multiple console screens and you have to switch back to your logging console to see it.
Hi,
I think when you remove the termination, the log will show again on the console. No?
Regards
Lunmin