How much size is required for download algorithm in code warrior hardware diagnostic tool?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How much size is required for download algorithm in code warrior hardware diagnostic tool?

ソリューションへジャンプ
1,867件の閲覧回数
karunakaranradh
Contributor IV

Hi,

 

I am planning to use the inbuilt 512KB SDRAM of T2080 as a target CPU in code warrior hardware diagnostic tool.

 

How much memory is required to download the algorithm to run the hardware diagnostic tool?

 

Regards

Karunakaran R

ラベル(1)
1 解決策
1,608件の閲覧回数
addiyi
NXP Employee
NXP Employee

The flash programmer algorithm required a maximum 30k.

Adrian

元の投稿で解決策を見る

2 返答(返信)
1,609件の閲覧回数
addiyi
NXP Employee
NXP Employee

The flash programmer algorithm required a maximum 30k.

Adrian

1,608件の閲覧回数
karunakaranradh
Contributor IV

Hi Adrain,

I configured the SDRAM in code warrior script  and set the SDRAM address as download algorithm address. With is configuration, i performed the 256MB of DDR3 memory test. it was working fine and faster also when compare with DDR3 set as download algorithm.

Thanks for your information.

Regards

Karunakaran R

0 件の賞賛
返信