How much size is required for download algorithm in code warrior hardware diagnostic tool?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How much size is required for download algorithm in code warrior hardware diagnostic tool?

Jump to solution
1,862 Views
karunakaranradh
Contributor IV

Hi,

 

I am planning to use the inbuilt 512KB SDRAM of T2080 as a target CPU in code warrior hardware diagnostic tool.

 

How much memory is required to download the algorithm to run the hardware diagnostic tool?

 

Regards

Karunakaran R

Labels (1)
1 Solution
1,603 Views
addiyi
NXP Employee
NXP Employee

The flash programmer algorithm required a maximum 30k.

Adrian

View solution in original post

2 Replies
1,604 Views
addiyi
NXP Employee
NXP Employee

The flash programmer algorithm required a maximum 30k.

Adrian

1,603 Views
karunakaranradh
Contributor IV

Hi Adrain,

I configured the SDRAM in code warrior script  and set the SDRAM address as download algorithm address. With is configuration, i performed the 256MB of DDR3 memory test. it was working fine and faster also when compare with DDR3 set as download algorithm.

Thanks for your information.

Regards

Karunakaran R

0 Kudos
Reply