Flash Programming Prerequisites

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flash Programming Prerequisites

跳至解决方案
1,895 次查看
deans
Contributor I

After a bit of trial & error I was able to do a flash dump through CodeWarrior. The first few attempts failed, apparently because the target system (5020DS) wasn't in the expected state. Resetting to U-Boot seemed make the CodeWarrior flash software happy.

 

So what is the expected state & how can I force the target into that state when I don't have U-Boot? (e.g., initial board bring-up)

 

Thanks.

标签 (1)
0 项奖励
回复
1 解答
1,640 次查看
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Dean,

For QorIQ processors with DPAA architecture (including P5020) it is a must to obtain valid RCW during power-on reset.

For systems with blank (unprogrammed Flash) there are two possibilities:

1) select a hard-coded RCW - refer to the P5020 QorIQ Integrated Multicore Communication Processor Family Reference Manual, 4.6.3.1 Reset Configuration Word Source and 4.6.4.1.1 Hard Coded RCW Options.

2) use RCW override feature of the CodeWarrior - refer to the CodeWarrior Development Studio for Power Architecture Processors Targeting Manual, 8.2 Using JTAG Configuration File to Override RCW.

Regards,

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,641 次查看
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Dean,

For QorIQ processors with DPAA architecture (including P5020) it is a must to obtain valid RCW during power-on reset.

For systems with blank (unprogrammed Flash) there are two possibilities:

1) select a hard-coded RCW - refer to the P5020 QorIQ Integrated Multicore Communication Processor Family Reference Manual, 4.6.3.1 Reset Configuration Word Source and 4.6.4.1.1 Hard Coded RCW Options.

2) use RCW override feature of the CodeWarrior - refer to the CodeWarrior Development Studio for Power Architecture Processors Targeting Manual, 8.2 Using JTAG Configuration File to Override RCW.

Regards,

0 项奖励
回复